When the Dimming function is not used, how to connect the circuit diagram
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If no duty cycle dimming is required and only 100% brightness is needed in application then PWM pin can be connected to VDDIO/EN pin directly, or other supply that allows at least 0.8 * VDDIO/EN level.
All other connections should be same as normal application.