This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22670: Minimum Load

Part Number: LM22670


Hi,

On the datasheet 7.3.5, minimum load is required as follows;

"A minimum load of about 5 mA is required to fully recharge the boot-strap capacitor in the minimum off-time."

Does the minimum load value depend on another condition(i.e. VIN, VOUT, fsw, etc...) ?

I would like to know if minimum load about 5mA is allowed on the below condition.

    VIN=12V, VOUT=3.3V, fsw=500kHz

Best Regards,

Kuramochi