I want to use the TPS92692 to drive 12 white LEDs from a supply between 9V and 36V. The calculator complains that I could exceed the 65V limit on the CSP / CSN inputs. Can I put the current sense resistor lower in the string at a location that doesn't reach 65V? How does this affect the OVP threshold? I would also like to be able to switch off 6 of the LEDs by shorting them out with a MOSFET. Will this impact the OVP threshold?