This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: How to determine max acceptable inrush current

Expert 3040 points
Part Number: TPS22810


Hi team, 

my customer is interested in TPS22810. they can know how to design inrush current in the application note in 10.2.2.3.

For example, 400mA is designed in this section. But why 400mA is used as example? 

If customer wants to set inrush current higher than 2A or 3A which is higher than max current, is this possible?

In the other word, how much peak current is acceptable on this IC when inrush happens? 

Regards, Naoki Yada