This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1: Vin - Vout range

Part Number: LM5050-1

Dear team,

 

we are doing some worst case analysis for a LM5050-1 design. Our datasheet sown a Vin-Vout range of 60mV max over full temp range and 12 V Vin range.

 

Furthermore we show 175mV in case we go up to 75V Vin.

 

  -

 

In case we wanted to design for guaranteed max gate voltage over full temp and high Vin, is our understanding correct that we have to design for 175mV Vin - Vout worst case then?

many thanks

Lutz