HI
I am designing a DC-DC buck where Vin= 12V, Vout=5V/5A with 0.1% load regulation. I am using LMZ12008 and design with web-bence. But in reality I am not getting 0.1% (5mv) load regulation at 5A, Voltage drops down to 4.884V.
1. Please suggest is there any way to improve the regulation or suggest any other part number to achieve such tight regulation.
2. Can I use series inductor at Vout pin of LMZ12008(as shown in the block diagram of datasheet) to improve the output filter.
Thanks.