This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: Can LM5145 work a output current sink?

Part Number: LM5145

Dear support member,

My customer used LM5145.

I'd like to use a output current sink operation at LM5145.
Is there no problem?

Does Over Current limit protection work?


Specification condition
Vin:24V
Vout:4V
Fsw:236kHz
Isink:4ADC

Best regard.
Bob Lee.