This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS561208: 7.3.1 Adaptive On-Time Control and PWM Operation

Part Number: TPS561208


Hi all

Would you mind if we ask TPS562108?

There is the description "7.3.1 Adaptive On-Time Control and PWM Operation".
Are these comments suitable for TPS562108?

What is Ton One-Shot used for on Functional Block Diagram?

Does it mean as follow;
"This one shot duration is set proportional to the converter input voltage, VIN , and inversely proportional to the output voltage, VO ,
to maintain a pseudo-fixed frequency over the input voltage range, hence it is called adaptive on-time control.
The one-shot timer is reset and the high-side MOSFET is turned on again when the feedback voltage falls below the reference voltage."

Kind regards,

Hirotaka Matsumoto