Other Parts Discussed in Thread: TS3USB221A
Hi,
As mr Hoferichter in this resolved post i have to use the same USB port for charging and communcation (Through Ft232) on a schematic for an embedded device.
After having carefully read the solution proposed to mr Hoferichter I ask myself the following question:
By putting two 150 Ohm resistor in line between the charger and the D+/D- bus would involve to sacrifice the DCP mode detection ?
If yes, what are the solution to save all charger type detection without disturbing communication?