Hi Team,
I got a question from the customer.
The calculation formula of fosc is described in the data sheet below.
fosc = 1 / Rt × Ct
However, I found a post that "fosc = 1.2 / Rt × Ct "is correct.
(Datasheet P19)
It is written that fosc = 20 kHz can be obtained with Ct = 0.001 uF and Rt = 50 kΩ.
I am confused which is right.
With information from customers,
Oscillation frequency (Used with Push-pull)
Rt: 6.2 kΩ ,Ct: 1000 pF ,Fosc = 1.2 / 2 (Rt * Ct)
Theoretical value: 96.77 kHz
Actual measurement value: 83.45 kHz
There was a big error.
I have been asked by the customer about the cause.
I appreciate your support.
Best rgards,
Kenji