This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2733: competing w/ PAM2841

Part Number: LM2733

hi all,

I need a boost led driver, 5V in, 29Vout @ 200mA.

something like the PAM2841.

I was looking w/ interest at LM2733, but didn't find any proofed design in LED driver config.

may you help me out?

thanks a lot in advnace

KR

Vincenzo

  • Hi Vincenzo
    You can use LM2733 for LED driver, the SCH is similar as PAM2841. but there is a problem.
    loss probelm:
    because LM2733 reference is 1.23V. so the R3 loss is 1.23*0.2=246mW
    PAM2841 reference is 0.2V. So the R3 loss is 0.2*0.2=40mW
    if customer can accept it, you can recommend LM2733.
    Thanks.
    Jing