Hi
The following use is assumed.
Two type of input sources: PC(USB2.0), Adapter
PC(USB2.0) : 5V/500mA(max)
Adapter : 5V/1A(max)
DPM function is not used.
Battery is Li-ion 1cell.
I think bq25606 can support it in the following configuration.
Could you please check it out?
If it is for PC(USB2.0) use, SDP would be detected by D+/D- detection function automatically and ILIM is set as 500mA.
If it is not for PC use, ILIM pin can be set as 500mA and ICHG as 1A.
Is it correct configuration? Please give me your view?
BestRegards