Other Parts Discussed in Thread: BQ24725A, , BQ24765
The BQ25708 data sheet is a bit weak in describing specific compliance with SMBUS 1.1  In our case, we've already invested time into a design using the BQ24725A to charge a smart battery pack, only to learn that it (1) loses all register settings when powered down and (2) crashes when the smart battery pack includes a packet error correction byte in its alert broadcasts.
Will the BQ25708 handle SMBUS PEC?  If not, can TI recommend a comparable charge controller that will give us the nice (seamless) buck/boost, operation without battery connected and the ability to respond to the smart battery pack?
Our pack is the excellent RRC2054.  Unfortunately we (and the manufacturer) cannot turn off the PEC as it's too deep within the protection device.