Hello,
LMG1205 has two VDD pins (A3 and C4), and two HS pins (C1 and D4). The datasheet shows A3 and C4, C1 and D4 are internally connected.
Do I have to connect A3 and C4 together externally? The same question for C1 and D4.
If it is not necessary to connect C1 and D4 externally, can I connect C1 to switch node, but use D4 for boot cap connection?
Thanks
Qian