Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62200 : Precision of the working at start up

Other Parts Discussed in Thread: TPS62200, TPS62240

My question is in the tittle.

I want to know what is the working of the TPS62200 for VI=0V to 2.5V? In my application, at start up, VI raised from 0 to 3.3V.

Thank you

  • The TPS62200 has an internal UVLO circuit.  This keeps the output off until the input voltage reaches some value between 1.5V and 2V.  This value is specified in the datasheet.  Once Vin passes this voltage, the part will start switching and the output voltage will begin to ramp up to the setpoint.  The device will operate at 2V input, but it is only tested and the specs guaranteed at 2.5V input.

    Does this answer your questions?

    The TPS62240 is a newer buck converter that you might take a look at.

  • Thank for your answer.

    It answers my question.