This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Boost converter: Vin = 60-75 VDC, Vout = 110 VDC, Iout = 6 A max.

Part Number: LM5022

I want to design a DC-DC boost converter with the following specifications.

Vin = 60-75 VDC,  Vout = 110 VDC, Iout = 6 A (max)

So far, I am not able to find any boost ic which meets above specifications.  So, I was thinking of using two LM5022 boost controller with 30-36 VDC input (i might be able to do that, as i am using two solar panels in series) and 55-60 VDC output and connecting the output in series. 

My question is, will this work?