Hi Team
we are using Bq21040 as a charger for charging 100 mAh battery in STBI_SSTD (smart sports training device)
As per my understanding device can be used for providing power to load as well as battery.
I have the following question
1) What will behaviour of the device if the battery is not connected?
2) As per my understanding, the device will still provide 4.1/4.2 volts with 1Hz (few hundred mV amplitude ) pulse superimposed over it. please correct me if it supposed to behave differently
3)How will device behave if charging current +load current is more than fast charge current?
3 b) if the device will reduce load current or charging current?
3c) if the device will reduce the battery current then how it will manage the constant current phase.