This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335-1A: Frequency compensation components

Part Number: TPS54335-1A


Hi,

The absolute maximum rating of the COMP pin is 3V MAX.

Can I use a capacitor with a rated voltage of 10 Vdc for these compensating capacitors?

Should I use a capacitor with a rated voltage of 50 Vdc to have a margin?

Best regards,
Seishin