I designed a DC/DC converter , 220V-550Vdc to 8Vdc. . Min load is 130mW, max load is 4200mW. The converter runs in burst mode up to 1.2W ( high ripple). I need to be in continuos mode at min load because the ripple in burst mode is not acceptable. How can I achieve this task ?
Transformer primary ind is 6mH, Np-s=16.666 ( primary to sec), Np-a= 10.9375 ( primary to aux), Ns-a= 0.65625 ( sec to aux)