This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576: getting 1.6 v output ......but using a fixed 5v lm2576

Part Number: LM2576


 the output for the circuit is 1.6 v but we are using a fixed 5v lm2576. the circuit we were following was given by lm2576 datasheet

  • Hello,

    There are many potential causes of an incorrect output voltage (instability, wrong component placement, layout problems, etc.). I want to understand more about your LM2576 design.  Could you share your PCB layout?  Also, are you seeing 1.6V output under all conditions (loaded, unloaded, across Vin range)?  Could you also share a waveform of VIN, VOUT, and SW under conditions where you see the 1.6V output?

    Best Regards,

    Katelyn Wiggenhorn

  • Hello,

    I am going to close this thread due to inactivity. Please feel free to ask additional questions if this issue persists.

    Best Regards,
    Katelyn