Part Number: TPS82130
Tool/software: WEBENCH® Design Tools
Hello,
I am wondering how the TPS82130 operates when a system initially powers up, and there are many circuits which begin to turn on as the output of the TPS82130 is high enough to enable everything else downstream. Lets assume the TPS82130 supplies some "5V Rail" voltage in a system, and there are many other circuits reliant on this Rail voltage. Each other circuit has a low steady state draw, but has some decent inrush current on startup. if the TPS82130 is not fully on yet, but is outputting >2.5V, which is enough to get other components started, then how does the TPS82130 act in this scenario?
Having a longer (~10ms) soft start on the TPS82130 is preferable, because there is some inrush current on the input as well. Am I forced to limit the current on the circuits downstream or stagger when these circuits power up?
Is there a risk of this chip being damaged in the high-load-demand-before-it-is-fully-on situation?
all I see in the datasheet is section 7.3.3, which still left me wanting some explanation in this scenario.
Thank you