Hi,
Please let me know whether there's any potential problem on below schematic.
1. OVLO/OVP : 4.6V~5.7V
2. Current Limit : 2.1A
TPS25944A_SCH_REV01_20180221C.PDF
thanks,
TS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please let me know whether there's any potential problem on below schematic.
1. OVLO/OVP : 4.6V~5.7V
2. Current Limit : 2.1A
TPS25944A_SCH_REV01_20180221C.PDF
thanks,
TS
Hi Rakesh,
thank for your comments.
I think that the design calculation tool of TI homepage is slightly different from the calculation.
TPS2594x-Calculation Sheet V1p0_PM550-SEC_1.xlsx
OVLO/OVP are configured correctly.
-> I have applied the EVM Board Value, but there is a difference in the TI Excel file. Please let me know which one is better.
DMODE pin 1 should be connected to GND.
-> thanks, I'll update the schematic.
To set current limit at 2.1A; choose R44 and R56 values as 42.3 k ohm
-> TI Excel Calculation Tool has 35.7K Ohm. Please check which one is right.

Is input reverse polarity protection needed? If no - D6, D9 can be removed.
-> Yes, I want to use input reverse polarity protection for this circuit.
thanks,
TS