This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM27402SQEVAL: LM27402SQ Circuit Output Fail Problem

Part Number: LM27402SQEVAL

Tool/software: WEBENCH® Design Tools

HI


I having trouble using the LM27402SQ/NOPB(WQFN Type)

I built a circuit to get 12V/4A output with 19V input. but It was fail.

I used TI Webench as a reference circuit, and the information is as follows.


When VDD is measured, a 0.7 V sawtooth waveform is output. I would like help.