I'm having problem in understanding how hybrid hysteretic mode explanation in the datasheet. Specifically on the value of AVDD and how does it help. Also, how does the "added frequency compensation affects" and VCR on the feedback.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm having problem in understanding how hybrid hysteretic mode explanation in the datasheet. Specifically on the value of AVDD and how does it help. Also, how does the "added frequency compensation affects" and VCR on the feedback.
Hi Ben Lough,
Thanks for the discussion about it. Another question however not relared on the title. On the given SIMPLIS Model of the UCC256301, can I use POP Trigger in the simulation and where should I connect the perturbation so I can see the Bode Plot of it?
Hi Carlo,
Apologies for the delay.To use POP, connect the input of the POP symbol to LO (it looks for the periodic operating point). The output of the POP symbol can be left unconnected. Next, place an AC source with low magnitude between VOUT and the top of the feedback resistor divider. Then place a bode plot symbol in parallel with the AC source you inserted. Here is an example of POP with the UCC25630x simplis model. UCC25630x_SIMPLIS_for_Carlo.zip
Best Regards,
Ben Lough