I realize TI makes great components, but you'll have to pardon me if I think this is a bit *too* great...
I re-implemented a reference design from the WebBench; however...the output voltage from the regulator chip is 10.9 volts...! A nice, steady 1.4A as well; the chip doesn't seem to have been damaged at all, and performs very consistently...but what I really needed was 3.3VDC.
I can provide the design I created, as well as the schematic, however I promise that I re-created it faithfully. The SMT soldering was right on, too. I did another assembly of the same board, and I'm consistently having the same problem: when these chips power on, they're kicking out over 10 volts.
Any ideas?
Here's the schematic. It's right from the WebBench calculator; my component values are those shown here:
I do note that the values chosen for 3.3 volts in the schematic differ from those shown in the datasheet as required to generate that voltage; are the divider settings that sensitive?