Part Number: TPS22953
Dear Community,
The data sheet for the TPS22953 appears to be missing some DC electrical specifications for the PG pin.
1) When the PG pin is driving low and sinking 400uA, (VIN and VBIAS between 2.5 and 5.5V) what is the maximum output voltage on the PG pin?
2) When the PG pin is high impedance and the pin voltage is externally pulled up to VOUT (VOUT, VBIAS and VIN between 3.4V and 5.5V), what is the maximum leakage current into the PG pin?
Thanks for your help.
Best regards,
Gavin.