This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: 4.1V charging instead of 4.2V - change parameters manually

Part Number: BQ27510-G3


Hello,

For a project, we charge the battery only at 4.1V to limiting the aging of the battery.

I use the bq27510-g3 gauge and do firstly the golden image at 4.2V.

Is it necessary to do a second cycle at 4.1V before generate the golden image or is it possible to change manually some parameters in flash ?

If yes which parameters ?

For our battery, the capacity at 4.1V is 90% of the capacity at 4.2V.

Should I change only the "DesignCapacity" or others parameters ?

Thanks

Stéphane