Other Parts Discussed in Thread: UCC256303, UCC256302, , UCC256301
Hi
According to the appnote "SLUA836–UCC25630x Practical Design Guidelines ", the HV pin is not suggested to connect to the DC input .However, in my application, it is possible that the client will use the DC source as the input. So my question is that can this function be disabled by some external circuit? I know there are two other devices(UCC256302 and UCC256303) among this UCC25630x series
which don't incorporate the X-CAP discharge function , however, due to the requirement of without using the PFC stage in my application, it seems that i have to choose the UCC256301or UCC256304 in terms of the need of wide-DC input range.
[My application background]
AC-DC converter:
1.INPUT: 176VAC~264VAC;OUTPUT:35V/3.7A (typ)/9A(peak)
2.Due to the low cost and small dimmension requirement , the PFC stage can not be added to the converter.
Best regards,
Rick