This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6C5912-Q1: About TLC6C5912-Q1 current value

Part Number: TLC6C5912-Q1

Hello Expert,

Thank you for your special support everyday.

I have two question about TLC6C5912-Q1.

1,What is the maximum Rate current ?

2,When outputting in parallel, what is the maximum current value that can be passed to pin 1?

Best,Regars.

Fukazawa

  • 50mA max current for each channel.

    First, TLC6C5912-Q1 outputs are just simple MOSFET, it is just simple ON/OFF control instead of constant current control, the current balance will be an issue for outputs parallel.

    Second, Vcc current can be found in the datasheet table easily.