Other Parts Discussed in Thread: SN74CBTLV3257, , TLV7031
Hello,
I use TLC59281 for controlling LEDs on my board, and I have an unused output that I'd like to control a local switch's SEL pin (SN74CBTLV3257). It looks like the output voltage on TLC59281 is variable depending on the current sink setting and the source. Ideally, I would simply size a pull-up resistor to 3.3V to match the programmed sink current (10 mA) and get V_OL < 0.5V when the TLC59281 turns the channel 'on'.
My concern is that the V_IL threshold of the switch is 0.8V max, so I need V_OUTn of TLC59281 to be below that with sufficient margin.
Have you used a pull-up resistor, or some other small basic circuit, to accomplish this 'logic output function' with current sink output LED drivers like TLC59281? If there's not an easy way to guarantee V_OUTn be < 0.8V with just a pull-up resistor, then I may need to look into using a small comparator like TLV7031 to interface between the LED driver and the switch.
Thanks,
Jonathan