This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: Inductance selection, TPS63060 or TPS63061

Part Number: TPS63060

The data sheet contains equations to bound inductance selection, and also contains suggestions. Aside from the mentioned issues with transient response, are there any functional issues associated with selecting an inductance greater than those in table 3? Such as 3.3uH or 4.7uH?

Thanks, Mark

  • Hi Mark,
    I do not expect any functional issues. My main concern is the higher chance of instability. But this can be addressed by simply increasing the output capacitance if needed.
    What drives the customer to use a higher inductance here?