I have developed a buck-boost using the web bench.Attached it the schematic from web bench.Only thing I have changed is instead of one RFBT resistor, I have used two ( one 10K RFBT2 potentiometer and other 100ohms RFBT1) and RFBB 536. So basically I can vary my pot speed from 1.4v-24V.Everything works fine for few days rather months, then suddenly voltage drops to the lowest.And when we check the continuity VOUT and AGND are shorted.I have had 5 of such cases.final 2.7Amp Web bench design.pdf