This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504EVM-674: Using the user guide.

Part Number: BQ25504EVM-674

I am currently undertaking some work in university using the BQ25504EVM, I am testing it in line with the User's guide. I am using a MyDAQ to test the circuit. When I go through the tests, I believe that it stays in cold start up mode, until I unplug the 10k resistor between STOR and GND, I only do this for a second and then plug it back in and it works as it should from the User's guide. My question is why does this happen and what is the relevance of having the 10k resistor on the charger output sense.

Another thing id like to ask is I have attached a normal capacitor to the Bat and GND (J2). and it just acts the same as if there is no storage element, I'm sure I am missing something straight forward, just I am hopefully moving onto a super cap after this.

Thank you in advance.

  • Hi, what's the behavior that cause you think the BQ25504 is in cold start up mode, the more detail description may help me understand what happend in your testing. And what's the 10K resistor number, R?
  • Hi,
    I had a Vin of 1V as stated in the test prcedure and noticed that it stuck at 0.9v. The reason i believe it is in cold start up is that VSTOR is stuck at approximately 0.9V. From my understanding this is the same as in cold start up, i may be wrong though. The resistor i am speaking about is an external resistor that the technical guide for the BQ25504EVM states to install for testing. It is between STOR and GND (J6-1 and J6-3) It is for the test procedures.

    Sorry for late reply, im based in the Cardiff and the weather has effected me quite severely

    Thank you.
  • Thanks for your clarification, I noticed you said you attached a normal capacitor/supercap after the BAT pin, how about the capacitance? I guess it more seems as the power-up with battery less than UV, there has a description that - For a battery that is more than a diode drop below 1.8V, the charger may get stuck in cold startup which is less efficient and would take longer to recover.
  • I didn't really get a proper chance to test out a capacitor due to university closing last week due to snow. The size of capacitor is not necessarily important, it is not for much more purpose than proving and showing the charge discharge curve. I am just trying to prove that it is possible currently. any recommendations for capacity would be helpful. I understand some of the theory behind the close start up, But I am still confused on the use of the resistor between STOR and GND, what would happen to the system if a lower resistance is used, or higher. With the 10k stated the procedures did not work until this was momentarily disconnected. But I have attached a smaller resistor and it works how it should be predicted.

    I intend to use a supercap after the proof that the system can work. I have been given a 0.9F 5.5v supercap, I think this is slightly overkill, but it was free so I would just like to see if I can also see the charge and discharge curves of this

    Thank you
  • You said you attached a smaller resistor and then it works, what's the value of this resistor?
  • So I changed the 10k for a 1k and it would start up straight away when doing the test procedures. Im wondering if it is to do with the limited current output from a MyDAQ, what is the job of this resistor I changed to 1k?
  • The resistor connect to the VSTOR pin acts as load. I suggest you try it again with a DC supply.
  • Thank You,

    I'm trying to Test if it is possible to power this IC using RF energy around 1-2GHZ. I have a rectifier system that I've tested but it is giving out a low current. So that's why I'm testing it using a power supply with a low current limit. I think it will take a long time to charge the super cap I have. But I just need to prove it can work