Tool/software: WEBENCH® Design Tools
Hi,
Please tell me about Webench simulation of TPS 54620.
When designing under the following conditions, the load transient oscillates, but why? The circuit constant has not been changed.
Why is it because the inductor placed by default is too large (56 μH), why is it optimized with this value? Optimizing efficiency with top priority will exceed 100 μH.
--------------------
Vin=12V,Vout=2.5V,Iout=0.3A
Load transient_TPS54620.pdf
--------------------
Best Regards,
Yuto Sakai