1. I am ready to use 12V power access, through the boost chip LM3478 to 16.8V, to the charging chip BQ24610. But in the process of testing LM3478, I needed a current of 3A, but I found that LM3478 was self protecting at 2A and began to fall. What is the reason for this?
2. I am going to make a portable products, before 24V buck to 12V, but MOSFET found serious fever, so then to change the 12V access, to boost the program, if there is any other better chip recommended, can finish my entire circuit?
Thank you