This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61194Q1EVM: What is the NT1?

Part Number: TPS61194Q1EVM


Hi all

In the <Using the TPS61194xEVM Evaluation Module User's Guide.pdf>,page 12 is said Evaluation Board Schematic,there is a NT1,what is NT1?And I can't find it on EVM?

I want to kown how to connect PGND with GND.

  • Hello,

    NT1 is not a physical component but a schematic symbol that allows for connecting ground (or other) nets together only at a specific place in PCB layout. PGND and GND should be considered as two different planes which will connect only at this point. This will keep the power ground (PGND) and noise-free ground (GND) separated.