Hi
I am designing a Wireless EV charger and after the rectifier I need a battery management circuit, so i wanted to buy one of BQ24450 and I had some question would appreciate if someone could help me.
1. has anyone used this IC with arduino to charge 12V lead acid batteries ? if yes then do i need to use I2C protocol. I saw in some websites that this IC is for 4 cell battery only so can i charge a 6 cell battery with it?
2. for 12V output how much input voltage i need for the IC, I mean does it boost the DC input or do i need an exact DC voltage at input for a certain output voltage?
thank you I woud appreciate if anyone could help me with this.