TPS3620-33 is being used to manage the input voltage to a 3.0V LDO. VDD input = 3.6V, Vbat input = 3.3V. Capacitance on TPS3620 Vout pin totals 33 mF. This design has been used for many years on multiple projects.
Customer reports that the LDO voltage will lose output sometimes and the suspicion is that some transient condition on the TPS3620 inputs is causing its Vout to drop. Its possible that the VDD or VBAT input is turning on/off at a 10Hz rate. Would one of the inputs switching like this or not being stable cause an issue with the TPS3620? Right now it is not known if the circuit is on long enough to fully charge the large output cap, so its possible Vout is still ramping when this happens.
Based on the TPS3620 data sheet, it seems Vout should always be connected to either VDD or VBAT. Are there any input conditions that could cause Vout to drop out?