Hi sir,
In my design, BQ25606 was used to charge a pack of lithium battery(2500mAh), which type is UR16650Z.
But I had encountered some issues now, that the status output is alternating between high and low levels during charging after a few hours, and i'm confused if the lithium is full charged. My circuit as followed, pls give some support.
(R10=240Ω,R11=0Ω,R12=430Ω,R13=0Ω) 0Ω is test resistance. And After plugging in 9V dc, Q1 has been on.
Regards,
Jenny