This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53667: TPS53667 PWM output when Enable is Low

Part Number: TPS53667


Is TPS53667 PWM output voltage level 1.7V when Enable is Low?

And I would like to know the measurement point of Datasheet Fig.109 and 110 ch3 SW1.
Is this PWM output? I thought so because it is about 1.7V when ENABLE is low.

Best Regards,
Kohei Sasaki