This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62088: derating Iout

Part Number: TPS62088


Hi,

Should I consider derating of I out with temperature?
If Yes, is there characteristic data on Iout derating versus temperature?
Or how much current can flow at 75 ℃ and 85 ℃?

Best Regards,
Yuto Sakai

  • Hi Sakai-san,

    Please contact me via a conversation, so that I can understand your specific application and use case. You seem to have a lot of questions on this device.

    There is a thermal image in the EVM user's guide which gives an idea about the temperature rise of the IC. As well, there is a derating note on page 4 of the D/S. But please contact me so I can understand your requirements.