This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Unable to edit Flash contents after IT_Enable command

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO,

Hi All, 

We are using BQ34z100-G1 & are trying to configure the parameters using BQStudio through EV2300.|
When I was in the middle of changing the battery parameters in the data flash, by mistake I clicked on IT_Enable command.
This changed the update_Status from 0x00 to 0x04. 

But after this, I am unable to edit any flash contents. Below is the snapshot of the error message. 


I assume that the monitor is not in sealed mode since SS bit is not set. 
I tried "Reset command" multiple times but it didn't help. 

Since the battery parameters are not completely correct, current optimization cycle cannot be successful.
Thus I want to stop this cycle & start fresh once I complete configuring all parameters. 
I am unable to do this, since its not allowing me to change the data flash registers. 

Please let me know, if there is a way to recover the battery monitor to normal working mode. 

Thanks,
Suresha