I have a customer who is using a LP38690 with Vin = 6.6V from a 400kHz switching power supply and Vout = 5.0V. They are using a 4.7uF ceramic capacitor on the input and both a 4.7uF, 0603 located right at the output pin of the part and a 47uF, 1210 located at the load which is an inch away through a .025 inch wide trace. Further away there are also some 0.1 uF’s and a few 100pF scattered about on the load line. The output load current varies between 20 mA and 450mA . I have ESR curves for the ceramic caps they are using .
The customer would like to know if this LDO would be stable in this configuration. The ESR curve for the 4.7uF output capacitor shows an ESR of over 100 m-Ohms at 400kHz and the 47uF which is an inch away shows about 20 m-ohms of ESR The data sheet would indicate this is not a problem as it mandates an ESR range of 5 - 500 m-Ohm. Please confirm.
If this circuit will not work as is, please recommend capacitor changes for the 4.7uF and 47uF capacitors that will enable stability across the load range.
Thanks, John Garrett, AFA