Other Parts Discussed in Thread: UCC28063A, UCC28061, UCC28810
Hi, team.
Can UCC29910A be used as the Buck type LED driver?
AC100-240Vin
~50Vout/3A Constant Current
Are there other suitable products?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The UCC29910A has been designed for the pfc stage in AC adapter type applications where the input voltage range is 90Vac to 264Vac and the output voltage is 84Vdc. It is most likely unsuitable for LED driver type applications since:
Many LED driver applications in the sub 150W power range utilize the flyback topology.
TI has reference designs that use the interleaved UCC28061 and UCC28063A
Please review 
For lower power level you could use the UCC28810 in a flyback application.
This is shown in PMP2698

Regards
John