Dear Ti,
I have faced some issues on in-rush current from your TPS2378 and would like to clarify further with you on the below.
E2ERESOLVE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti,
I have faced some issues on in-rush current from your TPS2378 and would like to clarify further with you on the below.
E2ERESOLVE
Hi Incognito,
Thanks for your questions.
1. Inrush current limit is that when PSE power on the PD, there will be a period that the PSE will charge the bulk cap at the back end of PD.
During this time, the current shouldn't be larger than the inrush current threshold of PSE. Here it is limited by PD internal hotswap FET.
Current limit is used to protect the circuit during normal operation which means the PD has passed the inrush stage and worked in fully on.
2. The inrush current limit is accomplished by internal circuit controlling the hotswap FET. This current is flowing from VDD - bulk cap -RTN- VSS.
3. The inrush current is due to charge the bulk cap. If the cap is increasing, the inrush current will be limited to 180mA max and the inrush period will be increased. So basically it shouldn't increase during inrush because it is limited by PD
4. Under normal operation, the inrush current will be limited to about 140mA (180mA max).
5. From IEEE802.3at standard, the inrush period should be smaller than 75ms. And the minimum delay from inrush to normal operation should be larger than 80ms.
6. If the bulk cap is very large, the inrush period will be long which will make PD hotswap FET heat up. But PD has thermal protection and will shutdown the device to cool down. It is not recommended that add too much bulk cap.
Thank you.
Best Regards
Jack Chen