One of my customers is using TPS40210 boost controller to convert 6.3V to 12V@1A. It appears this device was removed from SwitcherPro from some reason. Therefore I must use manual calculations. Equation 60/61 per datasheet did not seem to work out for me. I calculated the comoensation network as R4=6.34K, C2=8nF, C4=33pF. 600kHz is used. 130uF Cout, 37mOhm. Can you confirm these values?
Thanks
Viktorija