Hi,
I have implemented circuit for battery charging as seen above.
Input voltage = 5V
Output Voltage measured = 4.2V which is connected to Single cell Li-ion 3.7V 2600mAh battery.
Case1:
Both LED's were ON during charging and LED1 went OFF at 3.65V after 2 hours.
Case2:
Voltage on ST2 (~PG) = 0.07V where LED2= ON
Voltage on ST1 (~CHG) = 2.5V where LED1 = OFF
During the second trial LED1 is showing OFF (but battery is charging).
Why I am not able to see LED1 indication as ON while charging during my second experiment?
Also at what voltage LED1 should turn OFF in CASE1 indicating it has entered termination charge state?
Thanks in advance.
Regards.
Rahul