Other Parts Discussed in Thread: BQSTUDIO, GPCCEDV
Hello,
I am configuring a SBS design. The designer of the product has left the company and I am here to configure the BQ4050 while discovering everything.
The product uses 4 cells of Li-Ion, connected in 2 pairs of 2, i.e. the Gas Gauge sees 2 cells.
After reading the docs (datasheet, sluuaq3.pdf, etc) I have a few questions:
- For the design parameters,(Design Capacity, Design Voltage), I suppose that I take the data directly from the battery spec ? If so, do those parameters refer to the overall pack or to a single cell ?
- I read here: https://e2e.ti.com/support/power_management/battery_management/f/180/t/584060?tisearch=e2e-sitesearch&keymatch=bq4050
about default OCV table. Where do I get this from ? Is this the parameter defaults according to sluua3.pdf ?
- Do I have to go through all the 500 parameters manually ? If I understand right, the GPC report will give me all the gas gauging parameters ? The calibration parameters are filled in during the calibration process ?
- To charge my batteries, the BQ4050 pulls the FET drives automatically depending on SOC, or do I always need to send the FET commands via SMBus ?
I add in my design :
Thanks in advance.
Frank