Hi! We are using TPS562201 in our product to generate +5V from a Lead-acid battery source (14.4V or less). While testing, I have discovered that, according to Maximum Absolute Ratings, any reversal in polarity is really destructive - immediately - no second chance - component blows away. But we need to take MAXIMUM advantage from this battery life in the 12V range (pre-Buck converter stage), so we need to have as minimal added voltage drop in the circuit as possible. I thought about using 2A 350mV Schottky Diodes as a protection, but their reverse current can rise up to 3mA on 15V range. Do you think this is enough protection or this level of reverse current (don´t have an idea how much voltage would this generate on Vin) can be also destructive so there is no suitable protection for this component? Thanks in advance.