Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO
Hi all,
I'm running into a problem submitting my bqStudio logs to the GPCTool and I'd like to determine what's wrong with the data I am submitting, if I need to re-take the data, and if re-taking the logs is necessary, what I was doing incorrectly for this set. I have attached the truncated (discharge only) data sets I am submitting to the tool, as well as the raw full charge/discharge logs from bqStudio.
The error I'm receiving back varies depending on the parameters in config.txt. I am either getting:
"Error: Fit did not converge. Check data format and test schedule. Make sure that rate and temperature range is realistic for the application. If data is correct, try to reduce range between SOCmin% and SOCmax%
Error: Fit failed due to data format issues. Check settings, data format and test schedule."
or:
"Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule "
Would anyone out there be able to point out if my data is problematic, and what I could do to correct it? The readings from the gauge itself appear to be accurate, as they match what I am seeing on the dummy load I am using to discharge the battery with, so I'm unsure where there could be an accuracy issue. The battery in question is a 25.6V, 3000mAh, LiFePO4 Battery with 8 series sets of 2 parallel cells (16 cells total).
Any pointers would be appreciated. Thanks,
- Kyle